AXIS#.SWLS.LIMIT#
Description
Sets the position value for a software limit switch, LIMIT0 or LIMIT1.
Examples
Usage
If only one limit switch is enabled, AXIS#.SWLS.EN = 1 or 2, then AXIS#.SWLS.LIMIT0 is the lower limit and AXIS#.SWLS.LIMIT1 is the upper limit.
If both limit switches are enabled, AXIS#.SWLS.EN = 3, then whichever switch is set to a larger value is the upper limit switch and the other switch is the lower limit switch.
Code
Axis 1 lower limit switch set to 1000 and upper limit switch set to 5000. Axis 1 home position is set and then both software limit switches are enabled.
-->AXIS1.SWLS.LIMIT0 1000 -->AXIS1.SWLS.LIMIT1 5000 -->AXIS1.HOME.SET -->AXIS1.SWLS.EN 3
Context
For more information on limit switches, refer to Limits.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | Position Units |
| Range | -9,007,199,254,740,992.000 to 9,007,199,254,740,992.000 |
| Default Value | AXIS#.SWLS.LIMIT0 = 0 |
| AXIS#.SWLS.LIMIT1 = 5760 | |
| Data Type | Float |
| See Also | AXIS#.SWLS.STATE, AXIS#.SWLS.EN |
| Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.SWLS.LIMIT0 | 0x500F | 0x3 | DINT | - | Position | RW | False |
| AXIS1.SWLS.LIMIT1 | 0x500F | 0x4 | DINT | - | Position | RW | False | |
| AXIS2.SWLS.LIMIT0 | 0x510F | 0x3 | DINT | - | Position | RW | False |